Part Number: LM2901
hi,
i wanted to ask about the output value status, when i put on the output pull-up (3.3V through 10kohm resistor), the +VCC of the device is 24V and the -VCC of the device is 0V.
for my understanding:
- if the + input larger then - input, then the output will be 3.3V
- if the - input larger then + input, then the output will be 0V
but, what happened if no pull-up placed on the output?
thanks,