Other Parts Discussed in Thread: LMP91000
I need to build a Potentiostat with CV, LSV, Amperometry functionalities. The applied potential ranges will be: ±10 mV, ±50 mV, ±100 mV, ±650 mV, ±3.276 V, ±6.553 V, ±10 V. Corresponding measured current range: ±10 pA to ±0.25 A. Can anyone please suggest whether LMP7721 is a suitable candidate for this purpose? What other components I need to look for? Any suggestion will be very helpful.