Hello everyone,
I have been working for quite a few days now on a simple project using the OPA549. I have already posted some issues regarding distortion in the post "OPA549 heat generation problem?" which I now consider to be resolved. I have now experienced a new problem related to the OPA549 when loaded, and was actually surprised to find no information about it on this forum nor on the web (as far as my search went). To illustrate the problem, I built a simple follower circuit as shown below :
I simulated this circuit with TINA-TI, which posses the model of the OPA549. I also built this circuit in practice and recorded the following waveforms :

Adding a 4.7 Ohms load gives the following result :

There thus seems to be a problem at the zero crossing. Things get even worse at 50 kHz :

Now, back to 20 kHz and adding an offset to the input signal, I measured :

Thus, it seems that the problem is related to the current at zero crossing on the negative slope. At first I suspected my circuit to have some defect or undesirable effect somewhere, but after testing out four independant Op-Amps from different wires and power supplies, I came to the conclusion that the problem might not be related to my design. I first noted the problem when the load was a simple snubber circuit (10 Ohms in series with 10 nF). The glitches (small but present) appeared just past the peak of Vout, exactly when the output current crossed zero.
Only a few days later did I simulate this circuit on TINA-TI and discover that the problem was related to the OPA549 themselves, and was in fact normal, but yet unwanted. The following graphs were generated from TINA-TI and the same circuit (see the first figure) :

These are literally identical to my measurements. I tried to design a compensative RC circuit to minimize this effect, as for capacitive loads, but couldn't succeed to a satisfactorily degree. There seems to be no indication about this effect on the OPA549 datasheet. As any of you ever encountered a similar problem before? Is there a way to obtain a clean sinusoïdal output at 20 kHz (and below) and full current with this Op-Amp?
Thank's for your help