Hi,
I have some questions relative to OPA551 amplifier.
We are attempting to heat sink the device by connecting the DPAK package TAB to -15VDC (so tab connected to same potential as pin 4), and I stumbled on this note – see below. In our present setup, the pin 4 (negative supply input) and TAB are both connected directly to negative rail.
Assuming that pin 4 is already connected to negative supply, is it acceptable to connect the TAB of the OPA551 to negative power supply rail without any loss in performance? If not can the TABs of multiple OPA551 devices be connected to each-other (in this case electrically isolated from negative supply… basically a standalone copper pour used to heat sink multiple devices).
Thanks,
David