Other Parts Discussed in Thread: TINA-TI, TLE2027, TLC27L2
Tool/software: TINA-TI or Spice Models
Hello,
I am using a TLE2027 op-amp in several places in one of our products. I would like to use a spice simulation of one or more of these circuits. The datasheet "SLOS192C− FEBRUARY 1997 − REVISED APRIL 2010" , page 33, contains a listing of a spice model which I copied from the datasheet into my spice circuit. I have also included it below. Unfortunately the TLE2027 model does not run because it is not complete. There are instances of a diode called 'dz' but there is no definition of what dz is. By contrast, there are also diodes called 'dx' and there is a line towards the end of the sub-circuit that defines what dx is.
If I edit the model to change all the instances of dz to dx, I can make the model run, but it doesn't match what was written in the datasheet! Is this hacked model trustworthy?
Is a more recent spice model of the TLE2027 available?
I tried looking at TINA for a spice model but when I opened up the TLE2027 component there I found a sub-circuit (.SUBCKT) for a TLC27L2. That doesn't look right. The TLE2027 has bipolar inputs and the TLC27L2 is CMOS?
Editted to add
Forgot the spice model:
.subckt TLE2027 1 2 3 4 5
*
c1 11 12 4.003E-12
c2 6 7 20.00E-12
dc 5 53 dz
de 54 5 dz
dlp 90 91 dz
dln 92 90 dx
dp 4 3 dz
egnd 99 0 poly(2) (3,0) (4,0) 0 5 .5
fb 7 99 poly(5) vb vc ve vlp vln 0 954.8E6 -1E9 1E9 1E9 -1E9
ga 6 0 11 12 2.062E-3
gcm 0 6 10 99 531.3E-12
iee 10 4 dc 56.01E-6
hlim 90 0 vlim 1K
q1 11 2 13 qx
q2 12 1 14 qx
r2 6 9 100.0E3
rc1 3 11 530.5
rc2 3 12 530.5
re1 13 10 -393.2
re2 14 10 -393.2
ree 10 99 3.571E6
ro1 8 5 25
ro2 7 99 25
rp 3 4 8.013E3
vb 9 0 dc 0
vc 3 53 dc 2.400
ve 54 4 dc 2.100
vlim 7 8 dc 0
vlp 91 0 dc 40
vln 0 92 dc 40
.modeldx D(Is=800.0E-18)
.modelqx NPN(Is=800.0E-18 Bf=7.000E3)
.ends