Part Number: LM675
Other Parts Discussed in Thread: OPA564, OPA544
Attached is a drawing of a section of the circuit which currently uses the LM675T. The op amp is attached to heat sink and dead bugged into the proper nodes on a vector board. Vsig is a sinusoid which will go as high as +/-0.5V and up to 1Mhz. If Voffset = 0, the crossover “hiccup” occurs, the hiccup is about 2 us. As the frequency is increased, it becomes more noticeable and the sinusoid becomes “less pure”. Frequency does not seem to alter the 2us crossover time. If DC offset (positive or negative) is added enough to where the AC signal doesn’t cross 0, the sinusoid looks great, no visible difference between the signal and the LM685T output. If increased up to 1.5-2A with a DC offset so there is no 0 crossing, and up to 200kHz and there isn’t any noticeable distortion in the output. Looking for an op amp, which has a minimal crossover time so up to 20Khz (more comfortable with 50-200kHZ max) can be achieved, < 1% purity error in the sin wave output.
Interesting instability, if a DMM is wired in series with the 1 ohm resistor load to measure the current, the LM675T seems to go nuts and gives a 2A DC output and gradually decreases, it also shows large amounts of noise added to the Vsig +in line. This behavior is the same whether the cap and resistor connector -in or +in are present or not. This behavior did not happen when OPA544 was used. This seems to be repeatable. The OPA544 does have about a 10us crossover hiccup though.