Part Number: OPA564
Other Parts Discussed in Thread: OPA548
I wish to use the OPA564 (or similar) in an application whereby it supplies power to a Device Under Test.
It is being used here in place of a regular DC/DC or LDO,
Using the op amp will allow me to inject "noise" wave-forms needed for testing the DUT.
The load will appear as 1-5uF (regular decoupling for the DUT power rail) plus the DUT itself (mainly resistive) and drawing about 200mA maximum (when voltage is DC).
Can I expect the op amp to be stable with this sort of load? I realize that overshoot with a step input may be large, but I will driving it with offset sinusoidal wave-form of varying amplitudes (100mV p-p) and frequencies (up to 3 MHz) and not steps.
I realize that the transient currents drawn during "noise" injection may exceed normal ratings of op amp, but I will be gating this on for only short periods.
Thanks, David