This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am giving an I/P is 2.5mV and the gain is 4.
I am expecting an output of 10mV. But I am getting an O/P of 3.2V.
May I know what happened. Please find the attached simulation result and file.
Regards
hariINA333_CS.TSC
Hari,
The minimum output voltage swing to negative rail is 50mV so it cannot go to 10mV you expect - see below.
Therefore, if you want to see 10mV at the output, you have to reference the output to a voltage at least 40mV above negative rail. In the example below I used the 900mV input common-mode voltage as a reference voltage, and the output became as expected 910mV (Vout=Vref+10mV).
Since the INA333 macro-model does not simulate voltage swing limitations as a function of gain, supply, reference and the input common-mode voltage, you need to download Instrumentation Amplifier Output vs Common-Mode Voltage calculator under following link: