This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA547: Two OPA547 shorted at their outputs

Part Number: OPA547

I have two OPA547 used as non inverting Amps. Both are running different output voltages,
may be one at 30V the other one at 5V.Both are hardware current limited to ~80mA by a config. resistor of 270k.

In that case one is working as source, here the 30V Amp the other one as sink (5V) (I think)

Now I shortcut both outputs.

What happens ? The 30V opamp I think should go into current limit , and what about the 5V Opamp ?

The essential question is: will this kill one of the Opamps ?