This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV2254: TLV2254 noise Vpp compared with TLV9064

Part Number: TLV2254
Other Parts Discussed in Thread: TLV9064,

dear all,

i'm in a project that need to amplify photodiode output current signal. after signal transfer from current to voltage, i need to amplify this signal multiply 300 through 3 OPA stages. 

I found for same schematic and same board but just replace OPA device from TLV2254 to TLV9064, the output signal will bring much noise. i compared input voltage noise density between TLV9064 and TLV2254, TLV9064 is better than TLV2254. But for input current noise density and Peak-to-peak equivalent input noise voltage from 0.1Hz to 10Hz, TLV2254 performance is better than TLV9064. 

I know photodiode output signal with a very low BW, so i want to ask which spec mainly influence my photodiode amplify output noise Vpp performance?

thanks so much.