Other Parts Discussed in Thread: TINA-TI
Hello, It's a closed-loop transfer system with a 10V/V closed-loop gain. if my output signal now meets the limit of the SR, the SR is enough, and SR=2 * Pi * f * Vop. If the differential signal input is small signal such as sawtooth wave of 100Hz 100mV. We can calculate the output accurately according to the open-loop transfer function and negative feedback parameters. If the differential signal input is large signal such as sawtooth wave of 100Hz 2V, can I calculate it according to the transfer function????
The transfer function of the operational amplifier is the small signal transfer function. Taking the three-stage amplifier circuit as an example, the larger the differential signal input is, the larger the charging current to the second-stage miller capacitor will be. The charging current can be expressed by gm (transconductance) *vin (input differential voltage). If it is a large signal, the charging current of the second level miller capacitor will be saturated. The charging current of 100Hz 2V and 100Hz 4V of the second level miller capacitor will be the same (right?)., now that it's not linear, what's the transfer function? So is my understanding right?