This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I created a linear power supply based on OPA549 (scheme below) and it would work perfectly if there wasn't be one problem. When I supply an amplifier OPA549 with -5V and 15V everything is ok. I mean that output voltage is direct voltage. When I supply it with -5V and 30V linear output changes to switching mode witch I saw on an oscilloscope ( also below ). I can see that an OPA549 is turning off and off the output with high freg. I think it might be an thermal issue but I did apply heat sink and radiator wchich is cooling an amplifier, so it shuldn't be problem witch this. It isn't problem witch supplying becouse I tried to supply it in 2 diffrent ways and result was the same. Did anyone has the same problem?
Hi Patryk,
and absolutely no capacitive load at the output? Then remove the Zobel network for a test. For very fast-slewing input signals (during a fast turn-on, e.g.) the Zobel network can cause an additional load current spike!
Are you sure that the OPA549 isn't heating up too much? What tells the ES pin?
Kai