This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I have a square wave of max 45Mhz, high & low (3.3V & 0V), coming from output of a programmable oscillator.
Need to convert into equivalent frequency buffered pure sine wave? Is there any ready opamp circuit which can do this?
I have seen this, but seems not buffered: http://www.learningaboutelectronics.com/Articles/Square-to-sine-wave-converter-circuit.php
Hi.
this is usually done by the help of a passive 7-pole RLC-low pass filter. Have a look into the datasheets of chips providing DDS (direct digital synthesis). There you will find example circuits.
Kai