This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using the circuit shown below. The problem that I have is it is unstable. With no input signal it begins to oscillate at the output of the IA at around 1Hz, Do you have any idea why it would do this?
kai klaas69 said:Hi Andrew,
with such a high gain the +2.5V reference voltage must be very well regulated, stable and clean. Any source impedance of this +2.5V reference voltage will be critical. How do you generate the +2.5V reference voltage?
Kai
Reference voltage.docxkai klaas69 said:Hi Andrew,
with such a high gain the +2.5V reference voltage must be very well regulated, stable and clean. Any source impedance of this +2.5V reference voltage will be critical. How do you generate the +2.5V reference voltage?
KaiHi Kai,see the attached doc. I use a voltage divider and buffer the reference voltage.
I have resolved the issue by lowering the gain of the INA333 and following OpAmp, so the total gain is 2000. I have shown some 5Meg feedback resistors which are part of the circuit in the attachment. I don't know if they could be the cause or if the circuit is just sensitive at high gain. Those feedback resistors are part of another chip that is coupled to this circuit.
The Tpad is connected to ground.
I will check the other pins if I see the oscillation again. Thanks for the tip
Hi Thomas,
correction to my previous statement, TPad is not connected to any potential.