This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LPV812: Merging two reference designs

Part Number: LPV812
Other Parts Discussed in Thread: MSP430FR2311, CC2652R,

Hi guys

I would like to ask/confirm if my circuit designs is workable.

I took reference from two designs,

1. MSP430FR2311 Microcontroller IR Reflection Sensing Reference Design(www.ti.com/.../TIDM-FRAM-IRREFLECTIONSENSING)

2. Always-on Low-power Gas Sensing with 10+ Year Coin Cell Battery Life Reference Design(http://www.ti.com/tool/TIDA-00756

Currently, I am trying to implement CC2652R instead of MSP430FR2311. And I need an additional TIA circuitry.

From the reference 1, I do not know which TI Amp do they use as it is internal built in.

So, I followed reference 2, and use the external TIA circuit. Will this work?

Reference 2 uses LPV812. However, should my feedback components be the same? or should i follow reference 1?

Any kind soul please help.

Thank you and hope to hear from you soon.

Regards

Daniel Lim