Other Parts Discussed in Thread: TINA-TI, , AMC1311
Tool/software: TINA-TI or Spice Models
Hello team,
I simulated AMC1311-Q1 with +1/-1 V sine wave. But why it shows normal operation?
As far as I know, input range of AMC1311-Q1 is -0.1V to 2V.
In datasheet, there are absolute input voltage, specified linear input full-scale voltage, Input voltage(absolute maximum ratings)
I can't understand what exactly the three terms are different. Could you please explain the difference and what is real input range of AMC1311-Q1?
Based on my knowledge,
input voltage: input voltage range which enables very basic operation, but cannot
specified linear input full-scale voltage: voltage range which guarantees
input voltage(absolute maximum ratings): break down voltage range (Device cannot be recovered)
Is this right?
One more thing, does AMC1311 TINA simulation model in ti.com mean AMC1311-Q1 or AMC1311B-Q1?
I heard the difference of two devices are accuracy related spec. Is this accuracy spec reflected in TINA simulation model?
Thank you.
Regards,
Oliver Kim