Other Parts Discussed in Thread: OPA837, LMH6609, OPA838
I am in a situation where I need to replace an obsolete op amp with a new op amp. I intended to use the OPA830 as this looks to be the best op amp as a replacement however during board test this op amp may see a differential voltage of +5V which is greater than the maximum stated in the datasheet. If the current is limited at the input will the op amp be protected from damage? If so is <30mA protection enough?