This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA2128: Regarding current consumption

Part Number: INA2128

We would like to ask you about the current consumption of INA2128.

What is the maximum current consumption when operating at a supply voltage of ± 6 V with a gain of 1.4 times and an input voltage of ± 2.5 V?

  • Hi,

    as the datasheet does not contain further details, I would assume the 1.5mA maximum supply current specification. See also the figure on page 5 of datasheet showing the temperature dependency of supply current. And, finally, add the load current.

    Kai