Other Parts Discussed in Thread: XTR111
Only the power supply+24V was input, and the Q1 generates heat on the board.It is very hot.
Is there a problem with the circuit?
Q1 uses BCP56.
XTR116 is used for 4-20mA.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thank you for your post. Is the Q1 BCP56 in the SOT-223 package? Can you share a picture of your layout? It's important for this package type that you use larger copper pads to reduce thermal resistance and improve power performance. You can read more about this in the following Application report: http://www.ti.com/lit/an/snva036b/snva036b.pdf
-Tamara