This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA828: Datasheet has Contradictory info regarding minimum supply voltage

Part Number: INA828
Other Parts Discussed in Thread: INA826S, INA826, , INA317, INA118, TPS60400, MAX660

Hi,

I'm trying to find what is the minimum required supply voltage for this component.

In one place of the datasheet it is stated as ±2.25, but in another place it is stated as ±1.5.

Which is it?

My application is to run this from a 3.7 V battery, and can in principle use either +3.7 V (minus some losses) or from a buffered mid-rail at ~ ±1.65 V.