This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
My customer is using AMC1200/AMC1301 to measure 5V bus. The divider resistor is 120k/2.4k. And 1200 works fine but 1301 may have some deviation. When changing resistors to 800/20, the result is good for 1301. My questions are below,
Thank you for your help here.
YES. But you means that 120k/2.4k and 120/2.4 will have the same result? Only need to add R3' on the input pin of VINN?
Hi Lin,
do both, keep the resistances of voltage divider as small as possible and add the compensation resistor.
See also here:
sbaa215.pdf
Kai