Part Number: LMH6518
Other Parts Discussed in Thread: OPA859, THS4541
Hi,
I am trying to find ways to interface a stage of two (pos & neg side) OPA859 used as buffers, with their CMV centered at GND, to a LMH6518 which requires a CM range of 1-4V.
Since OPA859 is not a rail-to-rail opamp, it won't work with the max OPA859 swing of about 3Vpp.
It could be done with a THS4541 (or another FDA) used as a CMV shifter but i do not want that because it would degrade noise performance since i am using 4-OPA859 in parallel (instead of one) to lower its' noise.
So one option, if applicable, would be to use LMH6518 under a split supply topology. Is that doable? Will the digital circuitry inside LMH6518 still be functional with a +3.3V supply rail?
I am not worrying about the output of the LMH6518 having a CMV ranging around GND since a FDA will be used to drive the ADC instead.
So is it possible to run LMH6518 with a split supply of +/-2.5V?
Thanks in advance
Manos Tsachalidis