Part Number: INA240
We are experiencing a peculiar offset problem on the INA240A3. The offset seems to be consistently 200mA (measured), 30mV voltage on pin 8.
We connect the device as shown below. In a “low power mode” the V3P3 voltage is disabled, but there is a battery connected at BUS.
Is there any issue with having a voltage present on pins 3 and 2 while pin 5 is un powered? The datasheet leads me to think it should be ok, but all the applications show the shunt downstream of a switch. In our case, the shunt is upstream of a switch.
I am thinking this could potentially be changing the input bias current somehow and causing an offset. We are not seeing this on every part, making it a harder problem to track..