Other Parts Discussed in Thread: OPA2830
This is George Zuk at the University of Pittsburgh.
Back in 2016 I was working with you about a getting a bunch of the LMH6612's from the same wafer due to this will be used in a radiation environment.
Well I may need some more probably the same qty. About 5K.
This is just preliminary information for now. I wouldn’t need them till say late 2020 or 2021. More like 2021. The final completed date is some time in 2024-25.
There’s still is a lot of meetings and discussions on using this circuit again. It wasn’t in the plans earlier, but now they are thinking this board make may be used again.
So I’m just gathering information for the meetings in the upcoming months, if it’s still an option to do.
I guess my question is will these LMH6612s still be in production till 2024-25?
Then if so we’ll require probably a whole wafer lot again if that’s still possible?