Other Parts Discussed in Thread: TLC2652,
Hi,
I am using the composite opamp with TLC2652 (chopper stabilized opamp) and THS4001 (High speed opamp).
If the input voltage is -5V from the battery V1 without the AC input, the expected output voltage is 2V since the gain of the circuit is 0.4.
I was able to measure the 2V if a decap of 6.8uF (polarized) is not added for THS4001 opamp power supply pins.
I am using a parallel combination of 0.1uF(ceramic) and 6.8uF (tantalum) at the power supply pins of THS4001.
With these two as decaps, my output voltage is 2.5V but with only 0.1uF decap, i am able to measure 2V.
What might be the reason for this condition.
Note: For TLC2652, only 0.1uF (ceramic) decaps are used.
Thanks
Pavithra Joshi