This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Mark,
I have submitted the required information for this request and am waiting for the results of the request. This typically takes 2 days to complete.
I will reach out to you once I have the results or within 48 hours, whichever occurs first.
Regards,
Daniel
Hi Daniel:
Thanks for support , I will inform customer and after get it will feedback soon.
Regards / Mark
Hello Mark,
I was expecting to hear back on my thermal data request by now, but have not. I will look into it again tomorrow and come back with an update.
Thank you for your patience.
Regards,
Daniel
Hello Mark,
Unfortunately, there seems to have been an issue with my request and it looks like I am going to have to submit a new one. I am not sure what occurred, but will ensure it does not happen again.
I sincerely apologize for the delay and thank you for your patience. I will try to see that the new request gets handled ASAP.
Regards,
Daniel
Mark,
I have re-submitted your request and expect to hear back next week.
Thank you for your patience.
Regards,
Daniel
Hi Daniel:
Need your help to push and speed up process it because of we are creating customer's P/N than get order , thanks a lot.
Regards / Mark
Hello Mark,
I have personally reached out to the individual pulling the information and have been told that this information will be available by the end of the week.
Regards,
Daniel
Hi Daniel:
As customer request , please help to confirm , could this parameter table update to datasheet ?
If not , could TI provide guarantee letter ? contact window ?
Regards / Mark
Hi Mark,
This type of a request requires work and approval from someone besides myself.
I've asked about this and will get back to you as soon as I hear back, ideally tomorrow.
Regards,
Daniel
Hello Mark,
Thanks for your patience. Here's what I've gathered:
It's important to note that thermal performance is not assured like specifications in the electrical characteristics table that are tested at final test. The same holds true for a letter. Thermal metrics in semiconductor data sheets are given under very particular conditions. For example, there are particular PCBs used as outlined by JEDEC (e.g. low-K 1s, high-K 2s2p) that are used to obtain these values. It is extremely unlikely that the JEDEC PCBs and the application PCBs are exactly the same. Therefore these values are best used as a relative measure of thermal performance. Here are a couple application notes that have additional information. Section 1 of the first reference may be of particular interest.
That said, while it is possible to update the data sheet with the desired information, the fastest and most efficient way to meet this requirement is to look for a newer device that has the desired information already in the data sheet.
So, there are a couple devices that I recommend for evaluation. First, the TLV376 is a production device that compares well with the OPA344, but it does have higher bandwidth (5.5MHz). If this is not an issue, I would check this device first. Secondly, the TLV9101 is also potentially a good replacement, however that device has a slightly higher max offset voltage (1.6mV) than the OPA344. I should also note that the TLV9101 is currently in preview, but when the data sheet is finalized it will have all of the desired thermal information. Finally, the TLV9101 is more cost competitive than the other devices.
I hope this helps.
Regards,
Daniel