This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7171: Using the LM7171 as an astable multivibrator with output questions

Part Number: LM7171

Dear Tech Support

I am interested in using the LM7171 designed as a high frequency astable multivibrator, similar to the illustration shown in the data sheet. My question is: there are

no known values attributed to the diodes and zener diodes mounted across the output? Are these set to limit the output swing or, are they there to keep the signal on

the output locked to the zero baseline? How are the values of these diodes determined? Lastly, it seems that the output is a triangle wave at half supply level? Will I

need a second op amp such as, an LM7171 to function as a high frequency amplifier and a wave conversion to a square output with 50% duty cycle?

Regards

Michael

Cayote11@gmail.com