Part Number: MULTI-CAL-SYSTEM
Other Parts Discussed in Thread: PGA308, , PGA309
I am now calibrating the PGA308 using MULTI-CAL-SYSTEM.
The voltage is read from the MULTI-CAL-SYSTEM Labview software using the HP34410A as an RS232 script.
The Keysight 34461A has a USB interface.
Can I replace the HP34401A (RS232) with the Keysight34461A?
What should I do if it is replaceable?