This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA149: INA149 Pin Clearance

Part Number: INA149

Hello,

In INA149 datasheet, I understand that 200V voltage difference can occur between pin 3-pin 4.

For example, pin3 is at 200V with respect to my GND, pin2 is at 195V with respect to my GND and my negative supply is connected to GND or -12V value.

From datasheet, I understand that it is appopriate, however from voltage clearance perspectives, if I apply 200V difference between pin3 and pin4, distance between pin3 and pin4 breaks voltage clearance rule for 200V.

So, how can I be sure that these voltage differences (200V or more) are verified with this devices ( with these pin distances) ?

Best Regards