Other Parts Discussed in Thread: OPA192
Hello,
We are trying to integrate the PGA205 IC in an amplifying circuit - the scheme is attached below.
We encounter issues from an unknown source, any help will be appreciated.
The circuit includes two parts of amplifying - first part is an op-amp switching sensor's current to voltage,
which output in scheme can be seen as "TP2". This part includes analog switches for changing the gain rate.
The output of the first part is driven to the PGA205, which outputs can be seen at scheme at "TP1".
The problem is that when switching PGA205 (by A0 and A1) it influences the first part of amplifying,
which seem to be due to some undesired capacitance.
Attached below are oscilloscope views at TP1 and TP2 points, where the top is TP2 (first part of amplifier, I to V), and the
bottom is TP1 (output of PGA205). As can be seen, when changing switch state at PGA205 also TP1 as well as TP2 change rate,
and the signal which should be a trapeze is distorted.