Hello,
Let me confirm, the LM324 datasheet says that ESD protection cells in IN+/- are available only on LM324K and LM324KA only.
LM324DR does not have any ESD cells, is that correct?
If that is correct, there is no large amount of leak current seen when the input accidentally pulled lower than -0.3V. Is this understanding correct?
Or is there any other expected abnormal mode concern in such abnormal case? (Of course, I understood we must keep -0.3V but I'd like to know it to assess for abnormal case risk.)
Thanks in advance.
S.Sawamoto