Other Parts Discussed in Thread: OPA333, LM5056A, AMC1300, INA240, INA293, INA3221
Hello,
I am attempting to meaure bus voltages up to +48V with INA220 using the 9.2.4 typical application note in the datasheet, page 28, figure 32. http://www.ti.com/lit/ds/symlink/ina220.pdf?ts=1588366555281
I see there is a user guide for the -48V application note, but could not find anything for the +48V besides figure 32 in the DS. I am trying to understand the relationship between the RSHUNT resistor and the RL resistor (shown as 100 ohms in figure 32). I do not see any equations that show me the relationship between these to feed into the V+ and V- on INA220 to determine the resolution.
Am I missing something here? It seems like basically, they are using a 24V Zener to clamp the voltage "seen" by the INA220 on Vbus, correct? What would be the resistor tying the OPA333 and 5.1V Zener to GND?
Any advice or another solution which I can use here for higher than 36V bus voltages?
Thank you.