This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Yuan,
This may be possible but we cannot guarantee the device behavior when operated in this way since it has not been fully tested. I spoke with a member of the design team and there are some concerns, especially with the common-mode output voltage. If you look at the device datasheet, you will see that the common-mode output voltage is typically 1.29V, but has a minimum of 1.15V and maximum of 1.45V. Any variation in common-mode output voltage would result in a direct offset error if sensing in a single-ended manner.
To summarize, operating the device from unipolar supplies is best and using an operational amplifier for level shifting and differential to single-ended conversions is best.
Please let me know if you have additional questions.