Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA835: OPA835 simulation

Part Number: OPA835
Other Parts Discussed in Thread: TINA-TI

Hello,

I want to use the OPA835 in a LTspice simulation. However the OPA835.lib file seem to be incorrect or is not understood properly by LTspice. Simulation throughs an error:

ERROR: Node U2:I21:1:102 is floating and connected to current source G:U2:I21:1:RA
ERROR: Node U2:I19:1:102 is floating and connected to current source G:U2:I19:1:RA
ERROR: Node U2:I19:1:302 is floating and connected to current source G:U2:I19:1:RC

u2:vprobe1: Missing value, assumed 0V @ DC
u2:vprobe2: Missing value, assumed 0V @ DC

Is there a fix?