Part Number: VFC110
Hello
We are going to use VFC110 as an F to V converter accepting Freq from 2 to 3 MHz.
We receive this Freq via FO Receiver AFBR 2624Z, wave shape by a Schmitt Trigger,
then differentiate to create a narrow Negative Going Pulse.
My Q;s are:
1. What is the Response time for the Internal Comparator " tres " in nSec?
2. The Max Neg going Pulse Width your Data Sheet recommends as 1/10th of the Min Cycle Time
in our case the Cycle Time would be 333 nS for 3 MHz, so a 33.3 nS would be the Max.
What is the Min Neg going Pulse Width reqd to Trigger the internal Comparator?
The Ckt is shown below:
Thanks in advance.