This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA333: output has large ripple

Part Number: INA333

Hi,

I'm using INAEVM-MSOP8 to test INA333 with below configuration. V+=3.3V, V- = 0V. REF=0.3V(not to GND shown in the picture), IN- to GND is 1.65V(add a 1.65V reference from IN- to GND), RG=536ohm, which sets GAIN=187.

when 2mV is added to IN+ to IN-, the output waveform is 

when 10mV is applied to IN+ to IN-, the output waveform is

We are sure the power supply, the REF pin is very stable. 

So why is there output ripple(about 190mV)?