I saw many potentiostat circuits on the internet that use these OP AMPS with unipolar power and claim to have negative drive voltages at the reference electrode. My question is if this is possible with unipolar supply voltage? I understand that this cannot be possible or am I wrong? According to my numbers, (Vwe-Vre) / 100 = (Vre-Vce) / 100, so Vce = 2Vre-Vw, where Vwe = Vref = 1.5 -> Vce = 2 * Vre-1.5 Also, (Vdac-Vref) / 30k = (Vre-Vref) 30k, where Vre = 2 * Vref-Vdac -> Vre = 3-Vdac Finally, Vce = 2 * (2 * Vref-Vdac) -1.5 -> Vce = 4.5-2 * Vdac; So I want to have voltages between -900mV and 900mV at the reference electrode, so the DAC would oscillate between 3.9V and 2.1V. this is correct? or I misunderstand the operation of the circuit? But is it possible that these op amps, with unipolar power supply, can give those negative voltages? I thought not, please help me.