Part Number: TLV3012
Other Parts Discussed in Thread: TPS3700EVM-114, , TPS3700
Hello,
I have enquired about using the TLV 3401 as an undervoltage battery monitor and an engineer suggested that I use the TLV3012 part. I have recently used the TPS3700EVM-114 module and I noticed that when I swap out R1 for 604k my device functions properly when there is no load or less than 1 ampere load. I am using the comparator output to trigger the enable pin of my regulator and disable its output when it reaches a voltage of 3.24V and my issue comes in when I apply a load of 1 A. The comparator would trigger the enable pin of my regulator earlier when loaded as opposed to when there is no load to it.
When using just the battery as a power source, I suspect that the voltage drop at the input of my comparator along with the voltage drop across the pullup resistor on the output is causing this so I am looking at implementing a push pull comparator to address these issues. Is my diagnosis of the issue valid and would swapping the type of comparator I am using to a push pull solve my issue???
Is there an evaluation module or through hole comparator I can purchase to test my theory??
Thanks,
Ibrahim