Other Parts Discussed in Thread: OPA192-Q1
I need Vo spec as MIN/MAX.
There is only Vo specification as TYP in the datasheet.
Could you please give me Vo spec over temp as MIN/MAX?
Regards,
Kasuya
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I need Vo spec as MIN/MAX.
There is only Vo specification as TYP in the datasheet.
Could you please give me Vo spec over temp as MIN/MAX?
Regards,
Kasuya
The linear output swing of any op amp is a condition used in AOL test and is a function of output current (Iout).
Thus, in the case of OPA192-Q1 the max/min linear output swing over -40C to 125C temperature is 300mV from either rail with 10k load (Iout~+/-1.8mA) or 600mV from either rail for 2k load (Iout=+/-9mA) - see below.