Other Parts Discussed in Thread: XTR106
Hi,
I am working with the XTR115 to develop a 4-20mA loop to transmit transducer signals to a primary processor. I am using a 220ohm shunt at the instrumentation input.
Per the TI implementation guide: https://www.ti.com/lit/an/sboa107b/sboa107b.pdf?ts=1607707923000&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FXTR115
I have added capacitor cap C7 (fig.1) across the input/output. I initially assumed this cap was to aid in developing a steady voltage across the in and output of the current loop/suppressing transient line voltages from EMI/RFI. There isn't any specific notes about choosing to implement cap C7.
However, with this cap in place (SMD, X7R ceramic, 10nF) I get massive (relatively low voltage spikes) common mode interference @around 20kHz. I am using a 120VAC medical-grade switching PSU in a relatively low noise testbench room. See my scope screenshot below. This is observing the V+ pin with respect to earth ground. I verified this switching resonance is a result of my sensor design. Probing the supply lines alone, when not hooked up to anything shows a "clean" DC +12V (my system voltage).
Removing 10nF cap C7 immediately removes the switching transients and shows a clean signal. However, in this configuration, anecdotally, it seems the sensor and current loop is more susceptible to environmental RF noise (Wifi etc.). Looking for some guidance as to what exactly this cap is doing and if/when it should be implemented.
Thanks