Other Parts Discussed in Thread: TRF37D73,
Hi gents,
I've got 2 questions related to the TRF37D73 :
- I would like to increase output power of a DECT module, this module got a maximum RF output of 23dbm ( according to regulation), but can be limited to any value.
For a specific application where we can overpass the limits we would like to reach 30dbm.
According to datasheet maximum input of the TRF37A73 is 10dbm, so if I'm planning to limit the RF output power to 10dbm and the TRF37A73 output should be arround 30dbm.
can someone confirm that it is feasible? DECT is using GFSK modulation can it affect the way the TRF37D73 works?
- As the same RF DECT module connection is used to transmitt and receive,I'm wondering if the TRF37D73 is blocking the signal catched by the antenna on the way back to the radio module?
thanks for your help
regards
Bruno