Other Parts Discussed in Thread: LM393
I want to make sure that the input impedance of the input pins is high enough that it won't be affected by the voltage divider circuit I have designed here in the attached snapshot.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Raj,
the input bias current of 100nA of LM393N causes a voltage drop of 0.1V across R9. I guess that's not what you want?
I would remove R9 and R10 and split R8 suitedly :-)
Do you need help with this?
Kai
Yes Sure..... I would like to install 0603 resistors hence I split the values accordingly. Please help me with suitable values. The powering points MC+ And MC- are at 530V maximum and I am controlling Precharge and Accumulator Isolation Relay with this circuit. LM393 should change logic levels at 90% of the Battery Voltage.
Hi Raj,
Depending on your desired resistor tolerance, I would suggest splitting R8 into resistances as close to a 2.45kOhm and a 24.54kOhm. (So maybe a 2.44kOhm and a 24.6kOhm?)
To maintain the 10/11 ratio of the voltage seen at the bottom of R7, the ~2.45kOhm should be placed on the top of the voltage divider and the ~24.54kOhm should be placed on the bottom of the divider and connected to GND.
The voltage across the ~24.54kOhm should feed the "NEG_A" input to the LM393.
Would you still like to implement external hysteresis?
Regards,
Joe