Part Number: MULTI-CAL-SYSTEM
Other Parts Discussed in Thread: PGA309
Does the temperature calibration for the PGA309, using the multi-cal-system, have to be in order? For example, if I want to compensate the sensor at -40°F, 23°F, and 85°F, do i need to go from cold to hot, or can I set the pre-cal file to start with room temperature first, then -40°F, then 85°F?
Why does the system only check the 50% SPAN point at the first temperature?
Regards,
Avi