Other Parts Discussed in Thread: LM2901
Hi Team,
My customer has the design which using two LM2901-Q1 as the current protection solution. Below is the schematic: The CSA is the detected signal from current sensor, and the plot upper left is the waveform of CSA. The red dot line represent the threshold for positive and negative period.
The U2106:3 is used for detect if Vcsa exceed Vp and the U2106:2 is used for detect if Vcsa exceed Vn.
My customer has the question that, how to calculate the resistor value for U2106:3 to set the Vth_high = 4.16V and Vth_low=3.88v as the hysteresis window.
Also, in this calculation, do we need to take the offset voltage, input offset current, or bias current into consideration?
Thank you!
Pin