Other Parts Discussed in Thread: OPA365, TINA-TI
Hello all,
Well, truly speaking,I don't have much knowledge in electronics ...
I just want to design a trans impedance amplifier that should detect APD currents from 0 to 10uA.
Well..it looks simple and I can google it ,grasp few knowledge about it or just pick up the design which was already done by someone else...
..I tried but here are my design challenges:
Photodiode : Avalanche PD with 50nA dark current and 5 pF input capacitance..APD is biased such that Cathode is connected to the +27V (to 30V even) and anode...to the input terminal of the opamp...
opamp: Should be single supply (positive )and maximum voltage should be applied is 5V..
Bandwidth required: 1MHz..
and the next stage of this TIA is a HPF and LPF (to allow frequencies from 80kHz to 1MHz. and again should be single supply 5V opamps with sallenkey topology.)...
Looks like a puzzle for me and I could not figure out the best solution so far...
So..can someone help me in choosing the right opamp and how can I design it (I mean...for this configuration, how can I go with inverting configuration since current enters is positive?) just have a look at the block diagram...(there is no 1K resistor )

Thanks ...