Other Parts Discussed in Thread: OPA549
Dear experter of TI
We want to enlarge the analog signal Vin 0~5V to Vout (-10~10V) with OPA549, and the maximal output-current is 7A.
The schematic is as following.
We connect the Vout to a TEC , the resistance of this TEC is 2 ohm, the other terminal of the TEC is connedted with GND.
We found a question. When we feed the Vin with 5V, The maximal current of the Vout is only 1A, Normally it should be about 5A.
Is there anything wrong with the above circuit?
Looking forward to your reply, thanks
SunnyZhang