This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMC6081: NC pin

Part Number: LMC6081

Hi,

Is the NC pin a pin to which nothing can be connected?(Pin1/Pin5/Pin8)

Is the NC pin connected internally?

I want to connect as follows.
●Connection
 V+ = +2.5V
 V- = -2.5V
 NC(pin1)= 0V
 Non-inverting input(pin3)= 0V

Is there any problem?

Best regards,
Seishin