This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

LM321LV: LM321LV output swing level

Prodigy 70 points

Replies: 1

Views: 47

Part Number: LM321LV

Hi,

I am planning to use LM321LV in my design. anybody please tell the output voltage swing level for V+ = 3.3V and V- = ground.

Regards

Dinesh

  • Hello Dinesh,

    If the load is low current then swing would be very close to 0V to 3.3V.  See figure 6 in data sheet and imagine that -2.75V is actually 0V and +2.75V is actually 3.3V. For higher output current, the output resistance will cause some voltage loss. Again refer to figure 6 and expect a somewhat larger slope because supply is 3.3V instead of 5.5V  

    Regards,
    Ronald Michallick
    Linear Applications

    TI assumes no liability for applications assistance or customer product design. Customer is fully responsible for all design decisions and engineering with regard to its products, including decisions relating to application of TI products. By providing technical information, TI does not intend to offer or provide engineering services or advice concerning Customer's design. If Customer desires engineering services, the Customer should rely on its retained employees and consultants and/or procure engineering services from a licensed professional engineer (LPE).

     

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.