This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ,
We checked the TLV320AIC3254 Application Reference Guide, the PGA gain is controlled by the AGC and cannot be controlled by ourselves..
Can you help check which of the following registers are invalid when AGC is enabled?
Page 0 / Register 83: Left ADC Channel Volume Control Register - 0x00 / 0x53 (P0_R83)
Page 0 / Register 84: Right ADC Channel Volume Control Register - 0x00 / 0x54
Page 1 / Register 59: Left MICPGA Volume Control Register - 0x01 / 0x3B (P1_R59)
Page 1 / Register 60: Right MICPGA Volume Control Register - 0x01 / 0x3C (P1_R60)
Thanks.
BR
Trevor
Hi,
If you enable the AGC, the built in AGC hardware will control the PGA gain automatically as its algorithm will adjust to meet the requirement accordingly.
On the volume control registers, you should be able to control even AGC is enabled - I have verified this on EVM.
Hi pdjuandi,
Thanks for your help, could you help to check the following thread:
TLV320AIC3120: AGC and digital volume control - Audio forum - Audio - TI E2E support forums
Regarding this thread, it seems that the volume can only be controlled by the DSP when the AGC is enabled.
BR
Trevor
Hi,
I think he was referring to controlling this through DSP not necessary meant only works with DSP.
Are you not able to write the volume register at all when AGC is enabled?
From my testing on EVM I can change that.
OK good that's what I was trying to understand, it might be the case but will check out on EVM and let you know.
Hi,
It's confirmed and tested on EVM the volume can't be adjusted when AGC is enabled.
See attached ppt.