This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3204EVM-K:  TLV320AIC3204EVM-K:IIC communication issues

Part Number: TLV320AIC3204EVM-K

Tool/software:

We use MCU to communicate with TLV320AIC3204EVM-K, and now we have a problem. We use logic analyzer to capture data and find that after powering up MCU and TLV320AIC320EVM-K respectively, MCU sends data to TLV320AIC320EVM-K through IIC. TLV320AIC3204EVM-K cannot receive data without doing any operation, but it can receive data and start working after repowering TLV320AIC320EVM-K. What is the reason? Could you help me answer it? Thank you.

Regards.

  • Hi,

    The AIC3204EVM comes with the USB-MODEVM on which the I2C host is resided, how do you interface with the MCU?

    Regards.

  • Hi,

    The connection between MCU and AIC3204EVM, as shown in Figure:

    Regards.

  • Do you have the USB-MODEVM powered? The picture shows only the connection, but the USB port is not connected.

    If you don't need the USB-MODEVM, you can use just the EVM with your MCU.

    Regards.

  • I did not use USB-MODEVM, MCLK, WCLK, BCLK, SCL, SDA are all provided by MCU, and I can see that there is no problem in the data transmission of I2C with the logic analyzer. The problem is that I have to power up EVM again before I can receive data, how can I make EVM receive data directly after MCU sends data? Instead of receiving data after repowering. Please help me analyze and answer, thank you very much!

    Regards.

  • This sound like, some parts/ICs are not powered initially.

    As you can see in the schematic, some powers of the device are given by the USB-MODEVM.

    My suggestion is you either power the USB-MODEVM or remove it and just use the EVM with your MCU directly.

    Please ensure all powers are powered and stable with RST pin low during power up. Once powers are up and stable you can release RST pin.

  • I found the problem, EVM is powered by pin 3 and 5 of P23, MCU is powered on, EVM is not powered on, SDA and SCL only 2.5V, both sides are powered on SDA and SCL voltage back to 3.1V, so if EVM is powered on again, the voltage of SDA and SCL will change, back to 3.1V communication success, EVM starts to work, What's going on here?

  • That's what I said, there are power needed in the USB-MODEVM. Please look at my suggestion above.

    Regards.